Configuring the supply fan - fan coil only - Johnson Controls - TEC312x-14-xxx - TEC3023-1x-xxx - TEC3322-1x-xxx - TEC3622-1x-xxx - TEC3022-1x-xxx - TEC3623-1x-xxx - TEC3323-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product
Thermostats > Fan Coil Thermostats > TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document type
Quick Start Guide
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028
On two-pipe or four-pipe fan coil units, three different types of supply fans are supported. These are single-speed fans, multi-speed fans up to three discrete speeds, and VSF using a 0 VDC to 10 VDC control signal and an optional binary on/off command.
Note: Fan control is not available in VAV mode.

For multi-speed fan control, you can adjust the point when the medium or high speed turns on. The fan speed is based on the load of the cooling or heating device, and is a percentage between 0 and 100. By default, the Med Speed On Cmd is 33% and the High Speed On Cmd is 66%. When you only use two fan speeds, set the High Speed On Cmd to 100% to disable the third speed.

For VSF control, the output is configurable for any range between 0 VDC and 10 VDC. The parameters are Start Voltage, Full Speed Voltage, and Minimum Command. Start Voltage is the voltage output at which the fan begins running, and Full Speed Voltage is the voltage output at which the fan reaches full speed. Minimum Command is the percentage of the range between the Start Voltage and the Full Speed Voltage. The fan does not go below the minimum command when the fan is turned on. By default, the Start Voltage is 2 VDC, the Full Speed Voltage is 10 VDC, and the Minimum Command is 20%.

When the variable speed fan is off, the FAN binary output is off and the voltage at the VSF output is 0 VDC. When the fan turns on, the FAN binary output turns on and the voltage at the VSF output begins controlling the fan. When the VSF is configured for reverse acting mode, when the Start Voltage is above Full Speed Voltage, the VSF output is set to 10 VDC or the Start Voltage minus 1 VDC, whichever value is the lesser, when the fan is turned off.