Menus and submenus - Johnson Controls - TEC3022-1x-xxx - TEC3023-1x-xxx - TEC312x-14-xxx - TEC3322-1x-xxx - TEC3323-1x-xxx - TEC3622-1x-xxx - TEC3623-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product
Thermostats > Fan Coil Thermostats > TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document type
Quick Start Guide
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028

In the following table, the * indicates that the menus depend on your configuration.

Table 1. Menus and submenus
Level 1 Level 2 Level 3
Setpoints Dehumidification Dehumidification
Cooling Valve Minimum Position*
Cooling Valve Starting Position*
Heating Valve Starting Position*
Coil Tempering Time*
Dehumidification Overcool Limit*
Chilled Water Supply Temperature Setpoint*
Temperature Occupied Cooling
Occupied Heating
Unoccupied Cooling
Unoccupied Heating
Standby Cooling
Standby Heating
Occ Setpoint Select
Heat Cool Setpoint Mode
Max Heating Setpoint*
Min Heating Setpoint*
Max Cooling Setpoint*
Min Cooling Setpoint*
Max Setpoint*
Min Setpoint*
Scheduling Schedule Options Set Schedule
Optimal Start Enable
Temp Occ Duration
Motion Sensor Timeout
Manual Occupancy Mode
Schedule Source
Display Settings Passcode Enabled  
Passcode*  
Brightness Setting  
Enable Backlight Timeout  
Units  
Time  
Time Zone  
Set Time Format  
Date  
Set Date Format  
Language  
Show Fan Button on Home  
Show Temp on Home  
Show Humidity on Home  
Show Off Button on Home  
Show Hold Button  
Show Setpoint on Home  
Show Alarms on Home  
Show Occ Status  
Show Unit Status  
Show Date/Time  
Setup General Setup Control Mode
Unit Enable
Fan Mode*
Max Setpoint Offset
Fan On Delay*
Fan Off Delay*
Frost Protection
Dehum Enable*
Unocc Dehum Enable
Dehumidification Sequence Mode*
Aux Mode
Load Shed Rate Limit
Load Shed Adjust
Fan Alarm Delay
Fan Alarm Action*
Fan Alarm Reset*
Fan Runtime Limit
Fan Runtime Reset*
Supply Air Temperature Alarm Offset
Supply Air Temperature Alarm Delay*
Unocc Low Speed Fan
Scheduled Circulation Enable
Scheduled Circulation Only when Occupied
Mininum Hourly Fan Runtime
Variable Speed Fan Circulation Setpoint*
Multi-speed Fan Circulation Setpoint*
Input Setup BI1 Config
BI2 Config
Supply Temp Sensor*
Supply Temp Offset*
Zone Temp Sensor
Zone Temp Offset
Humidity Offset
Reset Sensors
For networked models:

Zone Temp Alarm Enabled

For networked models:

Zone Temp Low Limit

For networked models:

Zone Temp High Limit

Setup (continued) Tuning Setup Temp Control Setup
Reset PID Tuning
Deadband*
Auto Economizer Tuning
Heat Prop Band*
Heat Integral Time*
Heat Process Range*
Heat Saturation Time*
Heat Time Constant*
Heat Process Dead Time*
Heat Period*
Cool Prop Band*
Cool Integral Time*
Cool Process Range*
Cool Saturation Time*
Cool Time Constant*
Cool Process Dead Time*
Cool Period*
Equipment Size
Network Setup FC Comm Mode
BACnet Instance ID*
For networked models:

N2 Address*

BACnet Address*
For networked models:

MSTP Baud Rate*

BACnet Encoding Type
BACnet/MSTP Communication Mode
For wireless models:

Pan ID

Equipment Setup General Unit Type
Valve Open Voltage
Valve Closed Voltage
Unoccupied Off Delay
Supply Fan Supply Fan Type*
Start Voltage*
Full Speed Voltage*
Minimum Command*
Medium Speed On Cmd*
High Speed On Cmd*
Reheat Reheat Installed
Reheat Min Damper Pos*
Reheat Fan Required*
Changeover Changeover Mode*
Supply Temp Type*
Changeover Setpoint*
Supply Temp Sensor*
Supply Temp Offset*
Trend EFF-ZNT  
EFF-SETPOINT  
EFF-ZNH  
B1 Status  
B2 Status  
EFF-OAT  
EFF-SAT  
FANSPD-S  
HTG-O  
CLG-O  
System Status Occupancy Source  
Unit Status  
Supply Air Temperature  
Changeover State  
Zone Temp Source  
Control Status Cooling % Command  
Heating % Command  
Reheat % Command  
Cool Stage 1  
Heat Stage 1  
Reheat Stage 1  
Fan % Command  
Fan  
Controller Info (Thermostat Info) Model Name  
Software Version  
Unit Name  
Device Name  
Device Description  
Commissioning Supply Air Temperature  
Heat Command  
Cool Command  
Supply Fan  
Aux  
Update View Version  
Load Firmware  
Restore*  
Backup*  
For wireless Models:

Network Status

Radio Code Version  
Radio PAN ID  
Active Channel  
Signal Strength  
Connection Status  
Network State  
IEEE Address  
Short Address