Location considerations - Johnson Controls - TEC312x-14-xxx - TEC3023-1x-xxx - TEC3322-1x-xxx - TEC3622-1x-xxx - TEC3022-1x-xxx - TEC3623-1x-xxx - TEC3323-1x-xxx - Proportional Fan Coil Thermostat - Thermostats - TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability

TEC3000 Series Proportional Fan Coil Thermostats Quick Start Guide

Product
Thermostats > Fan Coil Thermostats > TEC3000 Series Networked and Wireless Proportional Fan Coil and Individual Zone thermostats with Dehumidification Capability
Document revision
G
Revision date
2024-03-08
docpartnumberlabel
Part No.
Part number
24-11353-00028

For networked models, locate the TEC3000 Series Thermostat:

  • On a partitioning wall, approximately 5 ft (1.5 m) above the floor in a location of average temperature, to allow for vertical air circulation to the TEC
  • Away from direct sunlight, radiant heat, outside walls, outside doors, air discharge grills, stairwells, and from behind doors
  • Away from steam or water pipes, warm air stacks, unconditioned areas (not heated or cooled), or sources of electrical interference
  • In a clear path between the integrated passive infrared (PIR) occupancy sensor, if equipped, and the space it monitors

For wireless models, also locate the thermostat:

  • Outside of a recessed area, metal enclosure, or shelving unit
  • On the same building level as the other wireless devices on the same personal area network (PAN)
  • At least 2 in. (51 mm) away from any metal obstruction
  • In the direct line of sight to other wireless devices on the same PAN. Signal transmission is best if the path between the TEC3000 and other wireless devices is direct as possible. Line of sight is desirable but not required. See Table 1 and Table 2 for the recommended and maximum distances.
  • Away from metal and large solid obstructions, that includes equipment rooms and elevator shafts and concrete or brick walls, between the TEC3000 and the ZFR182x or ZFR183x Router/Repeater or ZFR Pro Coordinator Radio
  • Within range of two or more wireless devices on the same PAN. Redundancy in the layout provides the best reliability in wireless installations
  • At least 20 ft (6 m) from a microwave oven

For integrated PIR models, make sure that the thermostat is located centrally, where occupant movement is frequent. Ensure that the unit is not blocked by a plastic tamper resistant enclosure, such as the GRD10A-608. The plastic enclosure blocks the occupancy sensing capability.

The use of insulating foam pads is necessary for installations where wiring passes through the wall to the thermostat.

For wireless models, the effective transmission range and distance for indoor applications vary because of wireless signal absorption and reflection due to metal obstructions, walls or floors, and furniture that is found in building interiors.

Note: Allow for sufficient clearance to insert a USB drive into the USB port
Important: Only connect memory devices to the USB port. Do not use it for charging external devices.
Table 1. Indoor line-of-sight transmission ranges ZFR182x
Range type Transmission distance
  WNC Coordinator Router, ZFR Pro Router/Repeater TEC3000 Wireless Thermostat
Recommended 50 ft (15.2 m) 50 ft (15.2 m)
Line of sight, maximum 250 ft (76.2 m) 100 ft (30 m)
Note: For more details on using ZFR Pro Series communication devices, refer to the WNC1800/ZFR182x Pro Series Wireless Field Bus System Technical Bulletin (LIT-12012356).
Table 2. Indoor line-of-sight transmission ranges ZFR183x
Range type Transmission distance
  WRG Coordinator Router, ZFR Pro Router/Repeater TEC3000 Wireless Thermostat
Recommended 250 ft (76.2 m) 250 ft (76.2 m)
Line of sight, maximum 1000 ft (308.4 m) 1000 ft (308.4 m)
Note:
  • Actual range depends on the site and installation conditions. See Technical Documentation for more information.
  • For more details about using ZFR Pro Series communication devices, refer to the WRG1800/ZFR183x Pro Series Wireless Field Bus System Technical Bulletin (LIT-12013553).
Important: ZFR182x Pro Series Wireless System compatible TEC30xx-1x-000 models and ZFR183x Pro Series Wireless System compatible TEC31xx-1x-000 models are not compatible with each other and cannot be used under the same PAN ID (network address).
Figure 1. Thermostat shown with occupancy sensor, dimensions, in. (mm)