See Table 1 for terminal identification.
Figure 1. Low-side switching on/off wiring diagram
Figure 2. High-side switching on/off wiring diagram
Figure 3. Low-side switched floating wiring diagram
Figure 4. High-side switched floating wiring diagram
Figure 5. Floating control (pressure-dependent VAV)
Figure 6. Floating control (pressure-dependent VAV with changeover sensor/switch)
Figure 7. Floating control (pressure-dependent VAV with changeover sensor/switch and
reheat)
Figure 8. Floating control two-pipe heating and cooling hydronic valve control fan coil
application
Figure 9. Floating control two-pipe heating and cooling hydronic valve control with
changeover fan coil application
Figure 10. Floating control (on/off two-pipe and four-pipe fan coil applications)
Figure 11. Floating control (floating two-pipe and four-pipe fan coil applications)
Figure 12. Floating control two-pipe heating and cooling hydronic valve control fan coil
application
Figure 13. Floating control two-pipe heating and cooling hydronic valve control with
changeover fan coil application
Figure 14. AUX contact wiring
Figure 15. Binary input wiring