Features and benefits - Johnson Controls - LIT-12013193 - TEC33xx-1x-000 - TEC30xx-1x-000 - TEC36xx-1x-000 - TEC31xx-14-000 - RTU Thermostat - Floating Fan Coil Thermostat - Proportional Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - TEC3000 Color Series Thermostats

TEC3000 Color Series Thermostats Product Bulletin

Product
Thermostats > Fan Coil Thermostats > TEC3000 Color Series Thermostats
Document number
LIT-12013193
Revision date
2022-06-30
Table 1. Features and benefits
Feature Benefit
Two configurable binary inputs Provide additional inputs for advanced functions such as remote night setback, service or filter alarms, motion detector, and door, window, or fan status.
Two or three configurable analog inputs Provide additional inputs such as remote relative humidity, remote zone temperature, zone carbon dioxide level, damper feedback, or outdoor air temperature to support advanced control strategies.
Field-Selectable BACnet MS/TP or N2 Networked Communication (TEC36xx-1x-000 models) Simplifies the upgrade from N2 networked communication to BACnet MS/TP networked communication without changing hardware.
USB port configuration Rapidly clone the configuration between like units through simple backup and restore features from a USB drive to reduce installation time.
Programmable in seven languages Provides English, Spanish, French, German, Italian, Dutch, Portuguese. Requires a downloadable language pack.
Backlit full-color liquid crystal display (LCD) Offers an intuitive color backlit display that makes setup and operation quick and easy. The new display features on all models and offers real-time control status of the environment in easy-to-read, plain text messages with an adjustable backlight that brightens during user interaction.
Configurable touchscreen UI Facility managers can limit the user interaction with the thermostat display based on specific energy policies.
Various models available Offers models in modern black (code: hex #2d2926 or RAL 9017) or white (code: hex #F4F5F0 or RAL 9016) high-gloss designs with or without the Johnson Controls logo.
End-of-line switch Simplifies the layout and installation of communication buses.
Mobile Access Portal (MAP) Gateway compatibility (MAP Release 4.0 or later) Configure remotely, view the equipment and control the conditions through your mobile devices.
Onboard occupancy sensor (TEC3x13-1x-000, TEC3x23-1x-000, and TEC3x31-1x-000 models) Provides energy savings in high-energy usage commercial buildings without additional installation time or cost.
Integral humidity sensor Monitors space humidity on all models. Activates dehumidification control on two-pipe fan coil units with reheat, four-pipe fan coil units with individual coils or single coil with heating and cooling valves installed, rooftop units with hot gas reheat, and rooftop units with an auxiliary dehumidifier.
Multiple fan configurations for fan coil equipment types Provide field-selectable single-speed, multi-speed, and variable-speed fan control capabilities.
Full line of remote TE-6300 Series Temperature Sensors (See Table 8) Support a wide range of remote temperature sensing needs from a single supplier.
Built-in schedule object Enables all wireless and wired models of thermostats to be scheduled as stand-alone devices; allows wireless and BACnet MS/TP models to be defined and adjusted through the building automation system.
Optimal start Allows each thermostat controller to anticipate the heating or cooling needs of a space by starting the equipment early enough to reach the setpoint at the beginning of the scheduled occupancy.
Auto-tuned control loops Reduce commissioning time, eliminate change-of-season recommissioning, and reduce wear and tear of the mechanical devices.
Load shed Commands a load shed input to offset the heating and cooling setpoints by a fixed amount on networked models. The change rate of the setpoints is adjustable. The load shed feature is in place to help satisfy the California Title 24 requirements that are defined in joint appendix JA5, section JA5.2.4 for demand signal response. The trigger for this event is defined in another controller and passed through the network command.
Scheduled circulation Runs the fan for a minimum duration per hour. If the minimum hourly fan runtime is not exceeded as part of normal HVAC operation, the fan turns on at the end of the hour for the length of time required to fulfill the minimum run time. The fan runtime calculation includes runtime initiated when the Fan Mode is set to On and other overrides. The fan does not turn on if the fan runtime is already longer than the minimum hourly fan runtime.
Demand control ventilation (DCV)
Note: DCV is applicable only to Model 3 (TEC3x3x-1x-000)

Modulates the damper to control the rate of outdoor airflow into the zone in order to maintain the zone CO2 value at the zone CO2 setpoint. The following variants of DCV are available: demand control ventilation, occupant sensor control ventilation, and epidemic control ventilation.

Occupant sensor control ventilation is a variation of demand control ventilation for zones where the zone occupancy is determined with an occupancy sensor.

Epidemic control ventilation removes pathogens from the zone through ventilation. The epidemic control ventilation feature takes priority over demand control ventilation and occupant sensor control ventilation. An economizer must be installed to enable the epidemic control ventilation feature. The minimum ventilation position for the economizer damper can be set between 0% and 100%. This applies to both occupied mode and unoccupied mode.

Important: The TEC3000 Series Thermostat is intended to provide an input to equipment under normal operating conditions. Where failure or malfunction of the thermostat controller could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the thermostat controller.
Important: Le TEC3000 Series Thermostat est destiné à transmettre des données entrantes à un équipement dans des conditions normales de fonctionnement. Lorsqu'une défaillance ou un dysfonctionnement du thermostat risque de provoquer des blessures ou d'endommager l'équipement contrôlé ou un autre équipement, la conception du système de contrôle doit intégrer des dispositifs de protection supplémentaires. Veiller dans ce cas à intégrer de façon permanente d'autres dispositifs, tels que des systèmes de supervision ou d'alarme, ou des dispositifs de sécurité ou de limitation, ayant une fonction d'avertissement ou de protection en cas de défaillance ou de dysfonctionnement du thermostat controller.
Figure 1. Thermostat shown without occupancy sensor, dimensions, in. (mm)
Callout Description
1 Security screw
2 Display
3 USB port