Applications - Johnson Controls - 24-10859-2 - TEC-WALLPLT - Fan Coil Thermostat - Network Thermostat - Wireless Thermostat - TEC-WALLPLT Wallplate

TEC-WALLPLT Wallplate Installation Guide

Product
Thermostats > Fan Coil Thermostats > TEC-WALLPLT Wallplate
Document type
Installation Guide
Document number
24-10859-2
Document revision
Revision date
2020-04-08

The TEC-WALLPLT Wallplate is designed for use with any Johnson Controls® TEC3000 Series Thermostat Controller, to retrofit an existing installation or conceal mounting surface damage. The base of the thermostat controller attaches to the wallplate first, and then the assembly is secured to the wall using field-furnished mounting screws and wall anchors (if required).