Mounting considerations - Johnson Controls - Part No. 24-11370-00005 - TE-63xL Stainless Steel Flush Mount Button Temperature Sensor

TE-63xL Stainless Steel Flush Mount Button Temperature Sensors Installation Guide

Product
Document number
Part No. 24-11370-00005
Document revision
Revision date
2021-04-07

You can mount the Stainless Steel Button Sensor in many different locations, such as in a cabinet, control panel, walls, or in a standard mounting plate. Use the spacer to insulate the stainless steel threaded portion of the sensor from any drafts or temperature changes in the wall. You can also use the spacer to insert the sensor into the wall.