Conduit mounting - Johnson Controls - Part No. 24-11370-00005 - TE-63xL Stainless Steel Flush Mount Button Temperature Sensor

TE-63xL Stainless Steel Flush Mount Button Temperature Sensors Installation Guide

Product
Document number
Part No. 24-11370-00005
Document revision
Revision date
2021-04-07

About this task

In the following task, use the 1 in. (25.4 mm) or 2 in. (50.8 mm) Delrin spacer.

Procedure

  1. Insert the two sensor wires through the top of the 1 in. (25.4 mm) or 2 in. (50.8 mm) Delrin spacer.
  2. Thread the 1 in. (25.4 mm) or 2 in. (50.8 mm) Delrin spacer onto the back of the sensor.
  3. Use crimp connectors or wire nuts to connect all the wires.
  4. Insert a small piece of foam or insulation into the bottom of the 1 in. (25.4 mm) or 2 in. (50.8 mm) Delrin spacer to better insulate the sensor.
  5. Insert the sensor assembly into the 0.5 in. (12.7 mm) conduit until it is flush to the end of the conduit as shown in Figure 2. You can gently tap the sensor assembly with a hammer to get it into the conduit.
    Figure 1. Conduit mounting
    conduit_mounting.png
    Table 1. Conduit mounting description
    Number Description

    1

    0.5 in. (12.7 mm) conduit