Series-parallel wiring - Johnson Controls - Part No. 24-4034-107 - TE-63xxP - TE-6300P - Temperature Sensor - TE-6300 Temperature Sensor

TE-6300P Series Temperature Sensors Installation Guide

Product
Sensors and Meters > Temperature Sensors > TE-6300 Temperature Sensor
Document type
Installation Guide
Document number
Part No. 24-4034-107
Document revision
R
Revision date
2021-02-26

To wire a duct averaging sensor, or another model in series-parallel configuration, see Figure 1.

Figure 1. Series-parallel wiring network
Note:

Always use sensors of the same value and type throughout the network.

CAUTION
  • Risk of Property Damage.
  • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
ATTENTION
  • Risque de dégâts matériels.
  • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.
Important: Use copper conductors only. Make all wiring connections in accordance with local, national, and regional regulations. Do not exceed the TE-6300P Series Temperature Sensor’s electrical ratings.