About this task
The retainer is a gray plastic tube approximately 1-1/4 in. (32 mm) long x 1/2 in. (13 mm) in diameter. Use the retainer to lock the sensor holder into the conduit box. Using the retainer prevents the snap finger from deflecting, locking the sensor holder into the conduit