Cutting the sensor probe - Johnson Controls - Part No. 24-4034-107 - TE-6300P - TE-63xxP - Temperature Sensor - TE-6300 Temperature Sensor

TE-6300P Series Temperature Sensors Installation Guide

Product
Sensors and Meters > Temperature Sensors > TE-6300 Temperature Sensor
Document type
Installation Guide
Document number
Part No. 24-4034-107
Document revision
R
Revision date
2021-02-26

About this task

This information applies to Duct and Well models only.

If necessary, cut the sensor probe at the wiring end using the following procedure:

Procedure

  1. Mark the required length, measuring from the end of the tube without leads. The final sensor probe length must be at least 3 inches (76 mm).
  2. Cut the probe using a tubing cutter with a sharp blade, as shown in Figure 1. Cut slowly, using minimal pressure to decrease burr size and help avoid damage to the leads.
    Figure 1. Cutting the Sensor Probe
  3. Slide the loose tubing carefully over the leads to remove.
  4. Insert the leads into shrink tube (included) or use other material to protect the leads from potential sharp edges where the probe was cut. (Heat the shrink tube using a heat gun.)