Mounting the Duct Sensor - Johnson Controls - Part No. 24-4034-107 - TE-63xxP - TE-6300P - Temperature Sensor - TE-6300 Temperature Sensor

TE-6300P Series Temperature Sensors Installation Guide

Product
Sensors and Meters > Temperature Sensors > TE-6300 Temperature Sensor
Document type
Installation Guide
Document number
Part No. 24-4034-107
Document revision
R
Revision date
2021-02-26

About this task

See Figure 1 and mount the sensor as follows:

Procedure

  1. Drill a 1-3/8 in. (35 mm) diameter hole at the desired mounting location.
  2. Use the mounting plate as a template to drill four 1/8 in. (3 mm) holes for the screws.
  3. Mount the probe assembly to the duct using the four screws provided.
  4. Pull the wires into the conduit box and snap the conduit box onto the sensor holder.
  5. Install the retainer into the sensor holder.
  6. Wire the sensor to the controller using the wire nuts provided.
  7. Reposition the cover and tighten the retention screws.