Important: Do not install the TE-6300P Series Temperature Sensor probe in
ambient temperatures beyond the specified -50 to 220°F (-46 to 104°C) temperature range.
Installing the temperature sensor probe in ambient temperatures beyond this range may
damage the unit and void the warranty.