Status Display Menu - Johnson Controls - 24-9890-1397 - T612DFH-4+PIR - T612DFH-4 - T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability

T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability Installation Guide

Product
Thermostats > Thermostat Controls > T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability
Document number
24-9890-1397
Document revision
B
Revision date
2021-01-07
Product status
Discontinued

The Status Display Menu displays during normal thermostat controller operation. This menu continuously scrolls through the following parameters:

  • Room Temperature
  • System Mode
  • Schedule Status (Occupied/Unoccupied/Override/Standby [PIR Models])
  • Applicable Alarms – The backlight lights up as an alarm condition appears.
Note: An option is available within the Installer Configuration Menu to lock out the scrolling display and show only the Room Temperature parameter.