Choose the appropriate sequence of operation using Table 1 or Table 2. The modes presented are user-dependent on the sequence of operation selected. For two-pipe applications using a changeover sensor, choose the selection option (0): Cooling Only. Changeover occurs between Cooling Only and Heating Only. See Figure 1 through Figure 6 for sequence of operation examples.
Selection Option | Control Curve | Terminal Numbers Used (See Table 1 and Figure 1) | |
---|---|---|---|
On/Off Control | Floating Control | ||
(0): Cooling Only | See Figure 1. |
10: Normally Open (N.O.) Cooling 11: Normally Closed (N.C.) Cooling |
10: Open Cooling 11: Closed Cooling |
(1): Heating Only | See Figure 2. |
10: N.O. Heating 11: N.C. Heating |
10: Open Heating 11: Closed Heating |
(2): Cooling and Reheat | See Figure 3. |
6 and 7: Reheat 10: N.O. Cooling 11: N.C. Cooling |
6 and 7: Reheat 10: Open Cooling 11: Closed Cooling |
(3): Heating and Reheat | See Figure 4. |
6 and 7: Reheat 10: N.O. Heating 11: N.C. Heating |
6 and 7: Reheat 10: Open Heating 11: Closed Heating |
Selection Option | Control Curve | Terminal Numbers Used (See Table 1 and Figure 1) | |
---|---|---|---|
On/Off Control | Floating Control | ||
(0): Cooling Only | See Figure 1. |
10: N.O. Cooling 11: N.C. Cooling |
10: Open Cooling 11: Closed Cooling |
(1): Heating Only | See Figure 2. |
8: N.O. Heating 9: N.C. Heating |
8: Open Heating 9: Closed Heating |
(2): Cooling and Reheat | See Figure 3. |
6 and 7: Reheat 10: N.O. Cooling 11: N.C. Cooling |
6 and 7: Reheat 10: Open Cooling 11: Closed Cooling |
(3): Heating and Reheat | See Figure 4. |
6 and 7: Reheat 8: N.O. Heating 9: N.C. Heating |
6 and 7: Reheat 8: Open Heating 9: Closed Heating |
(4): Cool/Heat Four-Pipe | See Figure 5. |
8: N.O. Heating 9: N.C. Heating 10: N.O. Cooling 11: N.C. Cooling |
8: Open Heating 9: Closed Heating 10: Open Cooling 11: Closed Cooling |
(5): Cool/Heat Four-Pipe and Reheat | See Figure 6. |
6 and 7: Reheat 8: N.O. Heating 9: N.C. Heating 10: N.O. Cooling 11: N.C. Cooling |
6 and 7: Reheat 8: Open Heating 9: Closed Heating 10: Open Cooling 11: Closed Cooling |