If the T612DFH-4 or T612DFH-4+PIR Thermostat Controller fails to operate within its specifications, replace the unit. For a replacement thermostat controller, contact the nearest Johnson Controls representative.
| Display | Function |
|---|---|
| Service | Indicates that there is a service alarm in accordance with the programmable Binary Input (BI2). |
| Filter | Indicates that the filter(s) is dirty in accordance with the programmable Binary Input (BI2). |
| Window | Indicates that an outside window or door is open and has cancelled the thermostat controller heating or cooling action in accordance with the programmable Binary Input (BI1). |