Repair Information - Johnson Controls - 24-9890-1397 - T612DFH-4 - T612DFH-4+PIR - T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability

T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability Installation Guide

Product
Thermostats > Thermostat Controls > T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability
Document type
Installation Guide
Document number
24-9890-1397
Document revision
B
Revision date
2021-01-07
Product status
Discontinued

If the T612DFH-4 or T612DFH-4+PIR Thermostat Controller fails to operate within its specifications, replace the unit. For a replacement thermostat controller, contact the nearest Johnson Controls representative.

Table 1. Display Messages
Display Function
Service Indicates that there is a service alarm in accordance with the programmable Binary Input (BI2).
Filter Indicates that the filter(s) is dirty in accordance with the programmable Binary Input (BI2).
Window Indicates that an outside window or door is open and has cancelled the thermostat controller heating or cooling action in accordance with the programmable Binary Input (BI1).