North American emissions compliance - Johnson Controls - 24-9890-1397 - T612DFH-4+PIR - T612DFH-4 - T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability

T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability Installation Guide

Product
Thermostats > Thermostat Controls > T612DFH-4 and T612DFH-4+PIR Thermostat Controllers with Fan Control and Occupancy Sensing Capability
Document type
Installation Guide
Document number
24-9890-1397
Document revision
B
Revision date
2021-01-07
Product status
Discontinued

United States

This equipment has been tested and found to comply with the limits for a Class A digital device pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when this equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area may cause harmful interference, in which case the users will be required to correct the interference at their own expense.

Warning (Part 15.21)

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

Canada

This Class (A) digital apparatus meets all the requirements of the Canadian Interference-Causing Equipment Regulations.

Cet appareil numérique de la Classe (A) respecte toutes les exigences du Règlement sur le matériel brouilleur du Canada.

Industry Canada Statement(s)

This device complies with Industry Canada licence-exempt RSS standard(s). Operation is subject to the following two conditions:

  1. This device may not cause interference, and
  2. This device must accept any interference, including interference that may cause undesired operation of the device.

Le présent appareil est conforme aux CNR d'Industrie Canada applicables aux appareils radio exempts de licence. L'exploitation est autorisée aux deux conditions suivantes :

  1. L'appareil ne doit pas produire de brouillage, et
  2. L'utilisateur de l'appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d'en compromettre le fonctionnement.