Features - Johnson Controls - LIT-1921580 - T-8000 - Element Controller - T-8000 Remote Element Controller

T-8000 Remote Element Controller Catalog Page

Product name
T-8000 Remote Element Controller
Document type
Catalog Page
Document number
LIT-1921580
Revision date
2020-01-06
  • proportional sensitivity or two-position action selected from a marked rail. The rail is marked DA (Direct Acting) and RA (Reverse Acting)
  • equipped with flexure levers to reduce hysteresis and friction
  • gage and set point dial are visible through the cover
  • designed for surface mounting
  • adjustable gain (proportional) or differential (two-position) by repositioning the sliding leakport