The T-8000 Bulb Element Controller provides proportional, two-position, direct action, or reverse action temperature control. The T-8000 is designed for applications which require the sensing element to be located where extreme conditions do not permit controller mounting or where operational adjustments to the controller would be inconvenient. This relay-type instrument is ideally suited for installations requiring the controller to be mounted on a local control panel.
Refer to T-8000 Proportional and Two-Position Remote Element Controllers Product Bulletin (LIT-7171280) for important product information.
Figure 1. T-8000 Bulb Element Controller