Description - Johnson Controls - LIT-1921600 - T-5220 - Pneumatic Temperature Transmitter - T-5220 High Volume Output Pneumatic Temperature Transmitter

T-5220 High Volume Output Pneumatic Temperature Transmitter Catalog Page

Product
Network and Communications > Temperature Transmitters > T-5220 High Volume Output Pneumatic Temperature Transmitter
Document number
LIT-1921600
Revision date
2020-01-09

The T-5220 High Volume Output Pneumatic Temperature Transmitter measures temperature in ducts, pipes, tanks, or other areas requiring remote temperature measurement. The T-5220 converts the temperature measurement to an air pressure signal transmitted to a pneumatic receiver, controller, or receiver-indicator. When used with a Dewcel® Dew Point Measuring System (purchased locally), the T-5220 operates as a dew point transmitter. The T-5220 is designed for applications that require a high output capacity, a high degree of accuracy, or a transmitter of industrial quality.

Refer to the T-5220 High Volume Output Pneumatic Temperature Transmitter Product/ Technical Bulletin (LIT-7171175) for important product application and single point of contact information.

Figure 1. T-5220 High Volume Output Pneumatic Temperature Transmitter