Temperature/RH Mode Selection - Johnson Controls - Part No. 24-10094-9 - Surface-Mounted NS Series Network Sensors with LCD

Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-9
Document revision
R
Revision date
2021-05-04

About this task

Temperature/RH models include a push button on the face of the network sensor to allow occupants to view the temperature and relative humidity of the zone. Pressing the push button toggles between temperature and RH on the LCD. The LCD defaults to temperature 5 seconds after the push button is released.

The NS-AHR710x-0 and NS-APR710x-0 models also have the capability to set the desired default display to either temperature or RH. Follow this procedure to change the default display on these models:

Procedure

  1. If the display backlight is off, press and release the push button to illuminate the backlight. If the display backlight is already on, proceed to Step 2.
  2. Press and hold the push button for 5 seconds to switch to the desired default display (either temperature or RH).
    Note: The desired default display will flash for 5 seconds. After the display stops flashing, the new default display is in effect.
  3. Release the push button; the desired display is now the new default display.