Network Sensor Addressing - Johnson Controls - Part No. 24-10094-9 - Surface-Mounted NS Series Network Sensors with LCD

Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Brand
Johnson Controls
Product name
Surface-Mounted NS Series Network Sensors with LCD
Document type
Installation Guide
Document number
Part No. 24-10094-9
Document revision
R
Revision date
2021-05-04
Language
English

Most network sensors have a default device address of 199 on the SA Bus. For averaging models, the sensor address must be set on the dual-switch DIP switch block on the network sensor Printed Wire Board (PWB).

Averaging models are shipped with both switches set to ON, resulting in a device address of 203. Device addresses can be DIP switch set from 200 to 203; see Figure 4 and Table 1 for more details.

Figure 1. Dual-Switch DIP Switch Block

Table 1. Network Sensor Addressing
DIP Switch Address Switch 2 Switch 1

200

OFF

OFF

201

OFF

ON

202

ON

OFF

203

ON

ON