Fan Mode Selection - Johnson Controls - Part No. 24-10094-9 - Surface-Mounted NS Series Network Sensors with LCD

Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-9
Document revision
R
Revision date
2021-05-04

Some models include a fan mode push button on the face of the network sensor to select the desired fan speed. Pressing the push button toggles the fan speed between AUTO-OFF-low-medium-high on the LCD.