°F/°C Temperature Mode Selection - Johnson Controls - Part No. 24-10094-9 - Surface-Mounted NS Series Network Sensors with LCD

Surface-Mounted NS Series Network Sensors with LCD Installation Guide

Product
Sensors and Meters > Network Sensors > Surface-Mounted NS Series Network Sensors with LCD
Document number
Part No. 24-10094-9
Document revision
R
Revision date
2021-05-04

Certain models include a °F/°C push button on the face of the network sensor to provide temperature scale options for display. Pressing the push button toggles the temperature mode between Fahrenheit and Celsius on the LCD.