Software Manager is a software application that manages licenses for Johnson Controls® software that is installed on the same machine. Software Manager installs automatically when you install software that uses Software Manager to manage its licenses. Follow the steps in this document if you need to install Software Manager separately from the licensable software. Refer to Software Manager Help (LIT-12012389) for more information about Software Manager.
Use one of the following methods to install Software Manager:
- One-click installation: if you want to install Software Manager with the default settings. See Installing Software Manager with the one-click method.
- Custom installation: if you want to install Software Manager in a customized location. See Installing Software Manager with the custom method.