Installing Software Manager with the one-click method - Johnson Controls - Metasys - LIT-12012388 - Software Application - Software Licensing - 4.0

Software Manager Installation Guide

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
Installation Guide
Document number
LIT-12012388
Version
4.0
Revision date
2024-10-08

About this task

Follow these steps to install software manager with default settings.

Note: You must install Software Manager on the same machine where you install and license your other Johnson Controls software.

Procedure

  1. Download the Software Manager installer.
  2. Browse to the location where you downloaded the Software Manager installer.
  3. Double-click SoftwareManager_x.x.x.xxxx.exe (where x.x.x.xxxx is the version number). If prompted, enter the administrator user credentials. The Software Manager Setup wizard opens.
  4. Click Install. A progress bar displays the progress of the installation.
  5. Click Finish when the installation is complete.