Document introduction - Johnson Controls - Metasys - LIT-12012388 - Software Application - Software Licensing - 4.0

Software Manager Installation Guide

Brand
Johnson Controls
Metasys
Product name
Software Licensing
Document type
Installation Guide
Document number
LIT-12012388
Version
4.0
Revision date
2022-05-20
Language
English

The Software Manager is a software application that manages licenses for Johnson Controls® software installed on the same machine. Typically, the Software Manager is installed automatically when you install software that uses the Software Manager to manage its licenses. Follow the steps in this document if you need to install the Software Manager separately from the licensable software. Refer to Software Manager Help (LIT-12012389) for more information on using the Software Manager.

There are two methods to install the Software Manager: