About this task
To complete an update, download the files you need for the update before you install the update.
- If a download process is in progress for any update.
- If a download process is paused for any update.
- If a download fails for any update, the user must cancel or complete that download to download other updates.
If you exit this application now, the in-progress download will be paused. Do
you still want to exit?
. You can click Exit
Now to pause the download and close the Software Manager, or
Don't Exit to exit the dialog box and the
Software Manager remains open. To download the files you need to install an update, complete the following steps:
Procedure
Download errors
About this task
If a download fails, the following message appears: Download
Failed
. To check the actual error message, hover on the
Download Failed
message or check Windows event viewer. See
Windows event viewer for more information.
If any download is in a failed state and the user clicks the refresh icon to complete a manual refresh, the update displays in a failed download state after the refresh also.
A download can fail when there is insufficient disk space, no Internet connection, or if proxy authentication is required. See Table 15 for more information. Click the refresh icon to start the download process again.