License information in the expanded panels - Johnson Controls - Metasys - LIT-12012389 - Software Application - Software Licensing - 3.0

Software Manager Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012389
Version
3.0
Revision date
2020-10-30

You can click the expand icon for a product panel to view its licensing details. Click Expand All to expand all product panels and Collapse All to collapse all product panels. For a product with one or more active or expired licenses, a tick icon appears in the expanded panel next to the top license. The license with the checkmark icon is the one currently shown in the License Inventory table. See Changing the top license in the License Inventory table for details.

Table 1. License information in the expanded panels
Section Description
Features Included

Displays a list of all features that are activated for a license.

Information includes the feature name, feature description, and feature version.

Active Licenses

Displays all currently active licenses.

Information includes license type, date activated, activation method, expiration date, product key, order number, and features. If the product has no active licenses, the following message displays: No active licenses. See License types for more information about license types.

Expired Licenses

Displays all expired licenses.

Information includes license type, date activated, activation method, expiration date, product key, order number, and features. If the product has no expired licenses, the following message displays: No expired licenses. See License types for more information about license types.

Deactivated Licenses

Displays all deactivated licenses.

Information includes license type, date activated, date deactivated, deactivation method, product key, order number, and features. A file icon appears for any licenses deactivated using the offline method. You click the icon to regenerate the license release file for that deactivation. See Regenerating a license release file. If the product has no deactivated licenses, the following message displays: No deactivated licenses. See License types for more information about license types.