Online machine - Johnson Controls - Metasys - LIT-12012389 - Software Application - Software Licensing - 3.0

Software Manager Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012389
Version
3.0
Revision date
2020-10-30

An online machine that runs the Software Manager automatically retrieves the most recent Machine Tag at the following times:

  • On application start-up
  • When the user manually refreshes the main window using the refresh icon of the Licenses tab. See Software Manager introduction.
  • When the user initiates an online activation
  • When the user opens the Machine Tag dialog box

For online machines that run the Software Manager, the user can complete the following actions using the Machine Tag dialog box:

  • View the complete Machine Tag name
  • Update the Machine Tag
  • View the last updated time stamp
    Note: The time stamp displays the date and time of the most recent update to the Machine Tag. For undefined Machine Tags, it displays as: Never(unavailable). If the Software Manager has never retrieved the Machine Tag, it displays as: Unknown.