Offline machine - Johnson Controls - Metasys - LIT-12012389 - Software Application - Software Licensing - 3.0

Software Manager Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012389
Version
3.0
Revision date
2020-10-30

For the Software Manager that runs on an offline machine, the Machine Tag (View-Only) dialog box appears when you click the Machine Tag link. The Machine Tag dialog box displays the current known Machine Tag. If the Software Manager has no Machine Tag data, it displays as: Undefined.

If the Software Manager cannot connect to the License Portal as the machine has no Internet connection, or the online connection setting is set to None (offline) the following message appears: Unable to connect to the License Portal. See Online connection setting for more information.