License deactivation after the System ID changes
If a machine's System ID changes, you cannot complete the deactivation of any licenses activated for the machine's old System ID. In this case, contact Johnson Controls sales support and request manual deactivation of the licenses to make them available for reuse. The following scenarios provide examples where this is necessary:
- Operating system (OS) change: After installing and licensing software, the machine is re-imaged with a different OS without first deactivating the software license. Request manual deactivation to use the license on the same machine with a different OS, or on a different machine.
- Hardware failure: After installing and licensing software, the machine's harddrive or motherboard failed and was replaced. Request manual deactivation to use the license on the repaired machine or on a different machine.
- VM configuration changed: After installing and licensing software on a VM, the VM's Disk ID or UUID is changed without first deactivating the software license. Request manual deactivation to use the license on the reconfigured VM or another machine.
- VM moved to a new host: After installing and licensing software on a VM, the VM is moved to a different physical machine. Request manual deactivation to use the license on the moved VM.
License deactivation when the machine is unavailable or non-operational
If a machine becomes unavailable or is no longer operational, you cannot complete the deactivation of any licenses on that machine. In this case, contact Johnson Controls sales support and request the manual deactivation of the licenses to make them available for reuse. The following scenarios provide examples where this is necessary:
- Theft or loss of machine: After installing and licensing the software, the machine is stolen or lost. Request manual deactivation to use the license on a replacement machine.
- VM deleted: After installing and licensing software on a VM, the VM is deleted without first deactivating the software license. Request manual deactivation to use the license on a different physical or VM.
License deactivation when the license is not listed in the Software Manager
If a license is not listed in the License Inventory within the Software Manager, you cannot complete the deactivation of that license. This occurs if the machine's System ID has changed or if the Software Manager cannot access the license data, for example, it is deleted, moved, or corrupted.
For the case where the Software Manager cannot access the license data but the machine's System ID is still the same, you can add a license back into the License Inventory by reactivating it on the same machine without deactivating first. This makes the license available for deactivation. For example, you may need to do this if you uninstall the Software Manager and then reinstall it in another location on the same machine.
For the case where the System ID changed, see License deactivation after the System ID changes.