Offline activation - Johnson Controls - Metasys - LIT-12012389 - Software Application - Software Licensing - 3.0

Software Manager Help

Product
Building Automation Systems > Authentication and Licensing > Software Licensing
Document type
User Guide
Document number
LIT-12012389
Version
3.0
Revision date
2020-10-30

An offline activation requires multiple steps that start in the License Portal and then continue in the Software Manager. Before you continue an offline activation in the Software Manager, you need the license activation file for the product. Start the offline activation and retrieve the license activation file from the License Portal using a machine with an Internet connection. If you cannot access the Internet on-site, you need to obtain this file before you get to the site and transfer the license activation file to the offline machine. You can only activate one license each time when you complete and offline activation.

You can access the License Portal at the following link: https://software.jci.com/licenseportal/#/login.

Note: See Related documentation and refer to the required License Portal Help for more information on how to start the offline activation and retrieve a license activation file from the License Portal.