The Software Manager's main window displays the Licenses tab by default. The Licenses tab displays the License Inventory table of licensable Johnson Controls software products. If more than one license exists for a product, the License Inventory table displays the top license. See Changing the top license in the License Inventory table for more information. See the following table for more information about the details shown and the user actions in the License Inventory table.
Column name | Description |
---|---|
Product |
Displays the product display name. This field may be blank if activation of the license occurs before installation of the product. |
Licensed Features |
Displays the number of activated features and the total features available. For example, 2 of 5. |
Expiring Soon |
Displays Yes with the Expiring icon if at least one feature of a license is expiring within 30 days, or No if the license is not expiring soon. |
License Actions |
Displays the Choose Actions menu, which includes
the following options:
Note: The available Choose
Actions menu actions depend on the status of the
license.
|
Click the Expand icon to display the features associated with an installed product. If you activate a license before you install it, only the activated features display.
Column name | Description |
---|---|
Feature Name |
Displays the name of the licensable feature for the product. |
Feature Description |
Displays a description of the feature. |
Version |
Displays the licensable version of the feature. |
License Type |
Displays the type of license. For no current
licenses, the license type column displays |
Status |
Displays the current licensing status for the product. Statuses shown include the following:
|
Expires On |
Lists the validity end date for the product's
current license. For licenses that do not expire, |