VAV unoccupied heating - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

This section details the VAV unoccupied heating setpoints and related data, inputs, outputs, and operation.

Setpoints and related data

The setpoints and related data include the following items:

  • VAV unoccupied heating enable (HtgUnocc-En) Yes
  • VAV unoccupied heating setpoint (VAVHtgUnocc-Sp)
  • Operational space temperature (OprST)
  • Off during unoccupied (OffDurUnocc) No

Inputs

The inputs include the following items:

  • 24 VAC to limit switch safety terminal LIMIT, LIM2, LIM3
  • 24 VAC to gas valve verification terminal MV, GV2, GV3

Outputs

The output for VAV unoccupied heating is 24 VAC from H1, H2, and H3 heat output.

Operation

The control must be in an unoccupied mode and not in morning warm-up mode.

If the operational space temperature drops lower than the VAV heating unoccupied setpoint, all heat stages energize with approximately 30 seconds of delay between stages.

Heat remains energized until the operational space temperature reaches the VAV heating unoccupied setpoint + 3°F.

Any time the control enters the heat mode, the VAV BOX contact closes.