Heating parameters - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document type
Technical Bulletin
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

The heating parameters include the following items:

  • Heating mode enabled for operation (Htg-En)
  • Number of heating stages installed (#HtgStgs)
  • Heating type (Htg-Type)
  • Fan on delay for heat (FanOnDlyHeat)
  • Fan off delay for heat (FanOffDlyHeat)
  • OA heating cutout setpoint (HtgOATCutout)

No heat setup

Heating enabled is set to off.

Gas heat setup

Heating enabled is set to on.

Number of heating stages is set to 1, 2, or 3.

Number of gas valves is set to 1, 2, or 3.

Heating type is set to staged.

Electric heat

Heating enabled is set to on.

Number of heating stages is set to 1, 2, or 3.

Number of gas valves is set to 0.

Heating type is set to staged.

Proportional/Hydronic heat

Heating enabled is set to on.

Heating type is set to proportional.