Network occupancy override timeout - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

If communications are lost from a BAS, the control should automatically revert to occupied. This can be accomplished using some type of watchdog timer on the BAS communication to the NetOCC point.

When this feature is enabled, if the BAS does not write to the NetOCC point within the timeout time (default 15 minutes; user configurable), the control will revert to the Occupied state.