Redline - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

In Title 24, Redline refers to minimum operating reserve that must be maintained at the power generating and transmission system. If you go below that line, it is a stage 3 emergency load shed, and instead of changing set-points, you have to shut the system off.

On the SSE control, this input is a network command that will set a 5 minute timer and turn off and lockout 50% of the capacity. On a 2 compressor unit, this would be compressor number 2. On a 3 compressor unit, this would be compressors 2 and 3. On a 4 compressor unit, this would be compressors 3 and 4. Each time a Redline flag is received (toggled), it will restart the 5 minute timer. When the timer expires, the control will resume normal operation.