Setpoints and related data
There are no setpoints or related data for direct load shed.
Inputs
The input is direct load shed (DirLoadShd).
Operation
If the direct load shed is set to yes, the compressors stage off for 5 minutes. After the 5-minute disable period, the compressors stage on and the communicated value returns to no.