Enabling Bluetooth communication - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document type
Technical Bulletin
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

About this task

The Bluetooth Low Energy (BLE) module resides on the SEC communication card. The BLE provides wireless Bluetooth connection to your equipment with the Connected Workflows for Technicians mobile application (CWa). Use the CWa to access your equipment data for commissioning, troubleshooting, and regular maintenance.

Procedure

Choose one of the following methods to enable Bluetooth communication:
  • Hold the UCB joystick in the down position for three seconds. The BLE module name and PIN appears on the UCB LCD screen.
  • Alternatively, navigate to the Controller > Bluetooth sub-menu. Set the BT-Ena parameter to True. Set the BT-Command parameter to Start.