Minimum position - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document type
Technical Bulletin
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

When the control is in the occupied mode and the FAN output is energized, the economizer is positioned to the minimum position setpoint unless another economizer function commands it open or closed.

When the control is in the unoccupied mode there is no minimum position.