Fixed variable (IntelliSpeed) - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

Setpoints and related data

The setpoints and related data include the following items:

  • Economizer damper minimum position low speed fan (LowSpeedFan-MinPos)
  • Economizer minimum position setpoint (Econ-MinPos)
  • FAN control type - fixed variable (FanCtl-Type)

Operation

This function uses the following parameters to determine the economizer minimum position:

  • Fan control type = fixed variable (FanCtl-Type)
  • Occupied: no heat or cool % command (FanOnly-%Cmd)
  • Occupied: one stage of cool % command (1ClgStg-%Cmd)
  • Occupied: two stage of cool % command (2ClgStg-%Cmd)
  • Occupied: three stage of cool % command (3ClgStg-%Cmd)
  • Occupied: four stage of cool % command (4ClgStg-%Cmd)
  • Occupied: one stage of heat % command (1HtgStg-%Cmd)
  • Occupied: two stage of heat % command (2HtgStg-%Cmd)
  • Occupied: three stage of heat % command (3HtgStg-%Cmd)

When the control is in the occupied mode and the FAN output energizes and the VFD output reaches 100%, the economizer damper position is the economizer minimum position setpoint.

When the VFD output reaches the lowest percent command of the parameters above, the economizer damper position is the economizer damper minimum position low speed fan.

When the VFD output is between 100% and the lowest percent command, the economizer damper is positioned proportionally between the economizer minimum position setpoint and the economizer damper minimum position low speed fan.

Note: To disable the fixed variable economizer minimum position reset, set the economizer minimum position setpoint and the economizer damper minimum position low speed fan to the same value.