Economizer loading - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

Setpoints and related data

The setpoints and related data is economizer loading enable (EconLoad-En) set to on.

Operation

The economizer loading function works only when one compressor is operating.

If the SAT is less than the SAT low limit setpoint and the operating OAT is greater than 60°F, the economizer output increases to control the SAT to the operating SAT setpoint +/-0.5°F.