Differential dry bulb - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document type
Technical Bulletin
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

A mode which compares the indoor dry bulb temperature to the outdoor dry bulb temperature in order to determine if economizer cooling is available.

Additional logic and configuration settings have been added to compare the Space Temperature to the Outdoor Air Temperature has been added. When the Outdoor Air Temperature is lower than the Space Temperature, economizer cooling is available. A new Enum set was required to make this change only on this platform. Default value will remain as “Auto”.