CV option A occupied - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

When free cooling is available and the operating space temperature is greater than the operating cooling setpoint, the dampers modulate to control the upper SAT setpoint +/- 0.5°F.

If the economizer output is at 100% for 5 consecutive minutes and the operating space temperature is 0.6°F or greater than the operating cooling setpoint, the staged percent command starts to increase and energizes compressors. See Table 1 for additional information.

As soon as the staged percent command begins to increase, the economizer remains at 100%. If the operating space temperature drops to less than 0.6°F above the operating cooling setpoint, the staged percent command holds the current value.

If the operating space temperature drops 0.6°F or more below the operating cooling setpoint, the staged percent command begins to decrease.

If the staged percent command remains at 0 for 5 consecutive minutes the economizer modulates to control to the upper SAT setpoint +/-0.5°F.