Auto - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

The control determines the type of free cooling changeover based on which sensors are present and reliable. Conditions include the following items:

  • Operational space temperature and operational outdoor temperature = dry bulb changeover
  • Operational space temperature, operational outdoor temperature, and operational outdoor humidity = single enthalpy
  • Operational space temperature, operational outdoor temperature, operational outdoor humidity, and operational space humidity = dual enthalpy
  • If the operational outdoor air temperature value is unreliable, free cooling is not available.