Air proving switch setup - Johnson Controls - LIT-12011950 - Building automation software - Smart Equipment Controller - 5.0

Smart Equipment Controls Sequence of Operation Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Smart Equipment Controller
Document number
LIT-12011950
Version
5.0
Revision date
2024-06-06
Product status
Active

Setpoints and related data

The setpoints and related data include the following items:

  • Air proving switch setup (APSSetup)
    • Constant volume
    • Variable volume
    • None
  • Fan control type (FanCtl-Type)
    • Single speed
    • Not used
    • Fixed variable
    • Variable speed

Inputs

The inputs include the following items:

  • Air proving switch (APS)
  • Duct pressure 0 to 5 VDC (DCT PRS)