Introduction - Johnson Controls - LIT-12013765 - Wireless field bus - Smart Equipment Control

Smart Equipment Control Wireless Installation Guide

Product
Controls > Smart Equipment Controls > Smart Equipment Control
Document number
LIT-12013765
Revision date
2021-02-17
Product status
Active

Smart Equipment Controls (SEC) is a unified platform for controllers in commercial unitary, chiller, and air handling products manufactured by Johnson Controls®. The product line introduces the Smart Equipment Controls unit control board (UCB) as the primary system control. The controller incorporates basic compressor protection, indoor blower control, and advanced features such as integration of ventilation control.

The SEC board provides the flexibility to communicate to a larger building management system using the following methods:

  • Wired BACnet MS/TP®
  • Wired Modbus® RTU
  • Wired N2
  • Wireless field bus

This guide focuses on the wireless field bus option and the steps necessary to perform the integration.