Applications to avoid using wireless - Johnson Controls - LIT-12013765 - Wireless field bus - SEC - UCB

Smart Equipment Control Wireless Installation Guide

Brand
Johnson Controls
Product name
SEC
UCB
Document type
Installation Guide
Document number
LIT-12013765
Revision date
2021-02-17
Product status
Active
Language
English

Locations or applications that prohibit cellular telephones or Wi-Fi systems are unsuitable for the wireless BAS products. Do not use the wireless products in applications that cannot tolerate intermittent interference or where the following conditions apply:

  • Critical control features would affect life safety or result in large monetary loss, including secondary (backup) life-safety applications.
  • Data centers, production lines, or critical areas would be shut down.
  • Loss of critical control would result from loss of data from humidity or temperature sensor communications WRZ Sensors report as infrequent as once every 15 minutes to conserve battery life. It may take up to 1 hour for the controller to detect the loss of a defective sensor.
  • Operation of exhaust fans or Air Handling Units (AHUs) would impair a purge or pressurization mode.
  • Missing data would invalidate reporting required by the monitored customer security points.